Maker.io main logo

Control Powerful Electric Skateboard E-Bike 350W DC Motor Using Arduino

42

2026-03-25 | By Ron Cutts

License: GNU Lesser General Public License Microcontrollers Arduino ESP32

In this tutorial, we are going to learn how to control a DC motor using Arduino and a DC driver BTS7960B.

The motor can be a 350W or just a small toy Arduino DC motor as long as its power doesn't exceed the BTS7960B driver's max current.

Watch the video!

Learn more about Visuino: What is Visuino

About the Motor

Rated output power: 350W. Rated voltage: 24/36V DC

Rated speed 2750 RPM.

No-load speed 3300 RPM

Full load current = 19.20A.

No-load current = 2.5A

Rated Torque: 1.11 N.m (11.1 kg.cm).

Stall Torque 5.55 N.m (55.11 kg.cm) Efficiency = 78%

About the Motor

About the DC Motor Driver BTS7960B

Specification:

Double BTS7960 large current (43 A) H-bridge driver;

5V isolated with the MCU, and effectively protects the MCU;

5V power indicator on board; voltage indication of motor driver output end; can solder heat sink;

Just need four lines from the MCU to the driver module (GND, 5V, PWM1, PWM2);

isolation chip 5 V power supply (can share with MCU 5 V); Size: 4 * 5 * 1.2 cm;

Able to reverse the motor forward, two PWM input frequency up to 25kHZ; two heat flow passing through an error signal output; isolated chip 5V power supply (can be shared with the MCU 5V); can also use the on-board 5V supply; the supply voltage 5.5V to 27V

About the DC Motor Driver Bts7960b

What You Will Need

  • Arduino Uno or any other Arduino board

  • DC Motor Driver BTS7960B

  • A DC Motor could be small or something more powerful, like in this experiment

  • Power supply for the motor

  • Potentiometer

  • 2X Button

  • Jumper wires

  • Breadboard

  • Visuino software: Download here

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

What You Will Need photo 4

What You Will Need photo 5

What You Will Need photo 6

What You Will Need photo 7

What You Will Need photo 8

The Circuit

  • Connect Arduino digital pin [3] to the BTS7960 driver pin RPWM

  • Connect Arduino digital pin [3] to the BTS7960 driver pin LPWM

  • Connect Arduino digital pin [4] to the BTS7960 driver pin R_EN

  • Connect Arduino digital pin [3] to the BTS7960 driver pin L_EN

  • Connect the BTS7960 pin VCC to the Arduino analog pin 5V.

  • Connect the bts7960 pin GND to Arduino Pin GND

  • Connect the power supply pin GND (-) for the motor to the BTS7960 driver pin B-

  • Connect the power supply pin VCC (+) for the motor to the BTS7960 driver pin B+

  • Connect the motor positive wire to the BTS7960 driver pin M+

  • Connect the motor negative wire to the BTS7960 driver pin M-

  • Connect the potentiometer pin OTB to Arduino Analog Pin A0

  • Connect the potentiometer pin VCC to the Arduino analog pin 5V.

  • Connect the potentiometer pin GND to Arduino Pin GND

  • BUTTON1: Connect pin 1 to Arduino pin 5V

  • BUTTON2: Connect pin 1 to Arduino pin 5V

  • BUTTON1: Connect pin 2 to Arduino digital pin 8 and to a 1kΩ resistor; connect the other pin on the resistor to Arduino pin GND

  • BUTTON2: Connect pin 2 to Arduino digital pin 9 and to a 1kΩ resistor. Connect the other pin on the resistor to the Arduino pin GND

The Circuit

The Circuit photo 2

Start Visuino, and Select the Arduino UNO board type.

The Visuino: https://www.visuino.eu also needs to be installed. Download the free version or register for a free trial.

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino, and Select the Arduino UNO Board Type photo 2

In Visuino Add & Set Components

  • Add "SR Flip-Flop" component

  • Add "Speed and Direction To Speed" component

  • Add "Dual DC Motor Driver 2 PWM Pins Bridge (L9110S, L298N, AM1016A, BTN7960/BTS7960)" component

  • Add "Digital (Boolean) Value" component

  • Select "DigitalValue1" and in the properties window set "Value" to True. This will enable the driver; setting it to false will disable the motor driver, and the motor will not spin

In Visuino Add & Set Components

In Visuino Add & Set Components photo 2

In Visuino Add & Set Components photo 3

In Visuino Add & Set Components photo 4

In Visuino Connect Components

  • Connect Arduino digital pin 8 to "SRFlipFlop1" pin "Set"

  • Connect Arduino digital pin 9 to "SRFlipFlop1" component pin "Reset"

  • Connect "SRFlipFlop1" pin Out to "SpeedAndDirectionToSpeed1" pin "reverse"

  • Connect Arduino Analog pin 0 to "SpeedAndDirectionToSpeed1" pin "Speed"

  • Connect "SpeedAndDirectionToSpeed1" pin Out to "DualMotorDriver1" pin "Motors[0] > In

  • Connect "DualMotorDriver1" pin "Motors[0] > Forward to Arduino digital pin 5

  • Connect "DualMotorDriver1" pin "Motors[0] > Reverse to Arduino digital pin 6

  • Connect "DigitalValue1" pin Out to Arduino digital pin 3 and digital pin 4

In Visuino Connect Components

In Visuino Connect Components photo 2

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Generate, Compile, and Upload the Arduino Code

Play

If you power the Arduino UNO module, the motor will start to spin; you can adjust the speed with a potentiometer or change the direction by pressing the buttons.

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project that I created for this. You can download it and open it in Visuino: https://www.visuino.eu

Downloads

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.