Liquid Cold Plates

Wakefield Thermal’s liquid cold plates are a natural evolution beyond air cooling

Image of Wakefield Thermal's Liquid Cold Plates 180 Series Wakefield Thermal's liquid cooling is a natural evolution beyond air cooling where either due to thermal or footprint requirements, the desired performance can no longer be economically met by air cooling.

There are many ways to accomplish liquid cooling, but the most common method is to have a plate with a flow path that moves liquid under the devices. After the heat is absorbed into the liquid, it is taken out of the plate and into the larger system. While water or water/glycol are the most common fluids used in liquid cooling, gasoline, oil, and refrigerant are other fluids that can be utilized.

There are lots of ways to construct a cold plate and the methods can be driven by the level of performance needed, the materials needed or the environmental requirements.

One construction method is to use a series of cross-drilled holes in a plate. The holes intersect in the plate to determine the flow pattern and unneeded patterns are plugged. This construction method can be cost effective, but the pattern is limited to straight lines.

Another method is to embed a tube in a plate by machining a groove in the plate. The tube can either be placed toward the top surface of the plate to provide better cooling to devices mounted on that surface, or it can be embedded further into the plate so that it cools devices mounted on both sides of the plate. This option provides greater flexibility, but the thermal performance is limited because of the surface area of the tube perimeter.

To get more performance, extended surface area in contact with the fluid is required and this leads to machined cold plates. The cold plate is constructed of a plate that has been machined to form some flow passages and then a cover is assembled to capture the flow. The extended surface area can be machined in place or installed by use of a piece of folded fin. The cover can be flat or be another machined plate. The method of assembly of the two parts can be done by gasket/screw, glue/screw, brazing, or welding and is dependent on the required performance and the requirements of the environment.

DigiKey offers standard liquid cold plates listed below. Please contact DigiKey for custom design assistance.

View More Types of Liquid Cooling Solutions

Features and Benefits
  • Compact and efficient cooling method
  • Quiet, reliable and leak-free
  • Compatible with water, glycol or other cooling fluids
  • Standard and custom designs available

Liquid Cold Plates

ObrazManufacturer Part NumberOpisDostępna ilość CenaWyświetl szczegóły
COLD PLATE HEAT SINK 0.084C/W180-10-6CCOLD PLATE HEAT SINK 0.084C/W32 - Immediate$246.41Wyświetl szczegóły
COLD PLATE HEAT SINK 0.041C/W180-10-12CCOLD PLATE HEAT SINK 0.041C/W13 - Immediate$345.93Wyświetl szczegóły
COLD PLATE HEAT SINK 0.084C/W180-11-6CCOLD PLATE HEAT SINK 0.084C/W18 - Immediate$444.02Wyświetl szczegóły
COLD PLATE HEAT SINK 0.041C/W180-11-12CCOLD PLATE HEAT SINK 0.041C/W17 - Immediate$616.51Wyświetl szczegóły
COLD PLATE HEAT SINK 0.02C/W180-11-24CCOLD PLATE HEAT SINK 0.02C/W10 - Immediate$611.45Wyświetl szczegóły
Published: 2014-11-03