Webinar - Enabling Sensor-Based IoT Application Development

Sensors come in endless configurations and sensing types. What they all have in common is the ability to convert real-world conditions into digital and analog signals that allow technicians and engineers to visualize and react to the data in real-time using IoT (Internet of Things) resources. The SensorTile.box PRO is an easy-to-use programmable wireless dev kit for assembling IoT solutions using remote sensor data and smart local processing. The ultra-low power STM32U5 is connected via the BlueNRG 5.2 SoC, offering a full set of motion and environmental sensors.

Americas Channel Marketing Manager Mark Hopkins and Product Marketing Manager Steven Bakker for STMicroelectronics guide participants through the attributes of STM32U5 and other recently launched STM32 ARM Cortex MCUs. Mark and Steven will discuss and demonstrate three powerful modes of operation: Entry Mode to use the existing applications provided out of the box with the ST BLE Sensor smartphone app, Expert Mode to create a custom operational mode via the app with no code required, and Pro Mode where pro users can program their custom applications, leveraging the STM32 Open Development Environment and ST function packs.

The half-hour online webinar takes place on Tuesday, May 21, 2024, at 11 AM CDT. Even if you are unable to attend the live session, please be sure to register so we can send you a link to the recording when it is complete.

Register here: https://event.on24.com/wcc/r/4580425/C65716BF3C0A49B270A9E8C8645A4018?partnerref=blog

Informacje o autorze

More posts by DigiKey Editor
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum