Power Resistor Selection Tips for Industrial Motor Drives

Przez: Kenton Williston

Przekazane przez: Północnoamerykańscy redaktorzy DigiKey

The increasing power density of industrial machinery raises the risk of nuisance tripping, overheating, and catastrophic failures that can halt an entire production line. To mitigate these risks while meeting efficiency requirements, designers need resistors that address multiple issues. Some must limit inrush or fault events, others must dissipate regenerative energy, and still others must provide reliable thermal performance in compact enclosures. 

In short, choosing the right resistor has become a crucial part of designing reliable industrial motor-drive systems.

This article highlights the challenges industrial machinery designers face and the merits of corresponding resistor technologies. It then introduces exemplary resistors from Ohmite’s broad lineup that designers can use to address these challenges in common braking and transient protection scenarios.

Pulse energy absorption for inrush limiting and surge protection

Industrial motor drives routinely subject resistors to transient high-energy events. The precharge stage of a variable frequency drive (VFD) is a good example. When this stage powers on, its DC bus capacitors present a near short circuit to the supply, producing a sharp inrush current spike. Without a current-limiting resistor in the precharge path, this spike can trip upstream protection or damage the drive’s insulated gate bipolar transistors (IGBTs).

Similar high-energy pulse demands arise in fault energy absorption, crowbar circuits, and power supply protection stages. In all these cases, a resistor must absorb a brief but large energy pulse without mechanical degradation, enabling this process to be repeated over many operating cycles.

Ohmite’s PulsEater A Series ceramic composite resistors are purpose-built for this role. Their non-inductive bulk ceramic construction distributes energy uniformly throughout the resistor body, reducing the risk of wire fatigue that can damage conventional wirewound resistors. That same non-inductive structure also helps reduce parasitic voltage spikes during fast current transients, which is useful in protection circuits where switching edges can be abrupt.

The A Series covers resistance values from 1.0 Ω to 15 kΩ, continuous ratings from 2.0 W to 5.5 W, impulse ratings from 1,000 V to 2,500 V, and single-impulse energy capacities from 250 J to 2,800 J. This range allows designers to match their selection to the bus voltage and energy profile of a specific protection circuit.

For example, the 3.3 Ω AY33GKE (Figure 1) can limit the peak inrush on a typical 600 VDC bus to roughly 180 A (I = V/R), depending on system impedance and capacitance. This is high enough to charge the capacitor bank quickly but low enough to protect upstream contactors and IGBTs. The 2,000 V impulse rating provides headroom well above standard industrial bus voltages, and the 1,400 J single-impulse energy rating gives ample margin for a typical charging cycle.

Image of Ohmite AY33GKE resistorFigure 1: The AY33GKE resistor uses a bulk ceramic construction to absorb up to 1,400 J of single-impulse energy. (Image source: Ohmite)

It is worth noting that the AY33GKE has a modest continuous power rating of 4.5 W. This is plenty for the target transient applications. For example, once a VFD precharge cycle is complete, the resistor will be bypassed and will no longer need to dissipate energy.

Low-inductance dynamic braking in compact drive enclosures

When a VFD decelerates a motor, the motor acts as a generator, feeding regenerative energy back into the DC bus. A chopper circuit shunts this energy to a braking resistor, switching the current on and off at high frequency. If the braking resistor has significant parasitic inductance, these rapid current transitions produce voltage spikes that can damage the chopper IGBTs. At the same time, modern control cabinets are shrinking, leaving designers with less physical space for bulky convection-cooled resistor banks.

The TAP800 series thick-film planar resistors address both concerns. The resistive element is built on a high-alumina ceramic substrate that is metalized on the bottom for efficient thermal transfer. The planar form factor offloads heat directly into a chassis or cold plate, enabling high-wattage dynamic braking in enclosures where a traditional convection-cooled resistor would not fit. This planar construction also minimizes parasitic inductance and capacitance, thereby stabilizing performance under high-frequency pulse loading.

The TAP800 Series covers resistance values from 1 Ω to 10 kΩ, all rated at 800 W continuous with proper heatsinking. This broad range enables a single-resistor platform to serve braking circuits across a wide range of drive voltages and power levels.

The TAP800K390E (Figure 2) is a representative example. At 390 Ω, it is rated for 800 W of continuous power dissipation when mounted to a liquid or air-cooled heatsink. The critical specification for dynamic braking is its 80 nanohenry (nH) inductance, which ensures that high-speed IGBT switching does not induce destructive voltage transients across the chopper circuit.

Image of Ohmite TAP800K390E thick-film planar resistorFigure 2: The TAP800K390E is a thick-film planar resistor designed for use with conduction cooling. (Image source: Ohmite)

The TAP800K390E also provides robust electrical isolation between the live DC bus and the grounded mounting surface. With a maximum working voltage of 5,000 VDC and a partial discharge rating of 4 kVRMS at less than 10 picocoulombs (pC), it is designed for long-term reliability. These specifications ensure that the insulation withstands the repetitive high-voltage stress and switching transients characteristic of modern industrial drives without degrading over time.

Heavy-duty dynamic braking for high-inertia loads

Some motor-drive applications place less emphasis on compact packaging and more on sheer energy handling. Examples include industrial cranes, centrifuges, and heavily loaded downhill conveyors, where decelerating the load forces the motor to act as a generator, returning large amounts of kinetic energy to the drive. In these cases, the braking resistor must withstand severe surges and cool quickly between cycles to avoid thermal accumulation.

Ohmite’s Corrib280 series resistors are designed for exactly this kind of high-current, low-resistance duty. The series comprises corrugated resistive wire wound on a tubular ceramic core and fused in place with a vitreous enamel coating. This construction serves several purposes: the ribbed wire increases surface area for faster heat dissipation; the ceramic core and enamel coating promote efficient heat transfer while improving mechanical durability; and the hollow-core structure enables airflow through the resistor body for passive cooling.

The Corrib280 series is available in continuous power ratings from 35 to 1,500 watts, with resistance values as low as 0.10 Ω on the 300 watt models. This gives designers considerable flexibility to match the resistor to specific bus voltages, braking currents, and physical space constraints.

The C300KR50E (Figure 3) is a representative example. It provides 0.5 Ω of resistance and a continuous free-air rating of 300 W. More importantly for braking service, the Corrib280 series is rated for overloads of 10 times nominal wattage for 5 seconds (s). For the C300KR50E, this corresponds to a short-term pulse up to 3,000 W.

Imaeg of Ohmite C300KR50E chassis mount-resistorFigure 3: The C300KR50E uses a corrugated resistive wire wound around a hollow core to maximize thermal mass and air cooling. (Image source: Ohmite)

Compact conduction-cooled braking and load resistors

Smaller machines, automated guided vehicles (AGVs), and control cabinet retrofits often require braking or load resistors in highly constrained physical spaces. In these tight enclosures, traditional free-air convection is frequently insufficient to dissipate heat. Indeed, the heat generated by a standard wirewound resistor can readily damage surrounding components. To address this, designers can employ conduction cooling to dissipate thermal energy into a machine chassis, a cabinet wall, or a dedicated cold plate.

Ohmite’s Arcol HS series resistors are engineered specifically for these scenarios. These wirewound resistors feature a finned aluminum housing with a flat mounting surface optimized for thermal conductivity to a heatsink. The family spans power ratings from 10 to 300 watts and resistance values from 0.005 Ω to 100 kΩ. For designs sensitive to parasitic inductance, non-inductive variants are also available.

Using conduction cooling, this architecture can achieve significantly higher power densities than traditional open-air resistors. For example, when mounted to a heatsink, the HS100 series can dissipate 100 W. In comparison, this same series is rated for only 30 watts without the heatsink.

The HS100 R47 J (Figure 4) is a representative part. At 0.47 Ω, its low resistance is well suited to the braking profiles of AGVs and small servo drives, where short, intense deceleration events are interspersed with longer run periods. The 100 watt continuous rating provides sufficient capacity to dissipate braking energy averaged over this type of duty cycle. Its finned aluminum housing is designed for heatsink mounting.

Imaeg of Ohmite HS100 R47 J chassis mount-resistorFigure 4: The HS100 R47 J uses a finned aluminum housing designed for mounting on a heatsink. (Image source: Ohmite)

Conclusion

Designers of high-power industrial machinery need to mitigate the risks of nuisance tripping, overheating, and catastrophic failures, while also meeting efficiency requirements. When chosen carefully to match the application, Ohmite’s resistor solutions address multiple issues, from mitigating inrush or fault events to providing reliable thermal performance in compact enclosures, achieving robust performance under harsh operating conditions.

DigiKey logo

Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.

Informacje o autorze

Image of Kenton Williston

Kenton Williston

Kenton Williston uzyskał licencjat z elektrotechniki w 2000 roku i rozpoczął karierę zawodową jako analityk testów porównawczych procesorów. Od tamtego czasu pracował jako redaktor w grupie EE Times, a także pomagał przy zakładaniu oraz prowadzeniu licznych periodyków i konferencji w branży elektronicznej.

Informacje o wydawcy

Północnoamerykańscy redaktorzy DigiKey