LEDs Offer Advantages in Industrial Communications
Przekazane przez: DigiKey's European Editors
2012-03-13
Optical rather than electronic communications are attractive solutions for designers of industrial networks and relatively low rate, short-range data networks such as in the automotive sector. LEDs are commonly preferred as transmission sources in such systems due to their low power requirements, specific wavelengths, small footprints, and long lifetimes.
Such critical networks must withstand the high levels of electromagnetic interference commonly found in industrial environments and vehicles. They also need to resist high temperatures, and environmental threats like dust and liquids and avoid the generation of electrical 'noise' that could either cause interference or explosions under certain conditions. These requirements make LEDs good choices for highly reliable communications.
In addition to their use in readouts and display backlights, LEDs are increasingly used for data transmission in industrial/automotive communications systems. The distribution medium is often Polymer Optical Fiber (POF) which, in contrast to copper, has the advantages of flexibility, electrical insulation, and high resistance to harsh environmental factors such as dust, water, high or low temperatures, and vibration.

Another increasingly important factor in the growth in demand for POF-based communications and the associated LED-based transmission technologies is the dramatic rise in the price of copper in recent years due to phenomenal demand for that metal in booming manufacturing economies in the developing world, especially China¹.
Advantages of LED and POF systems
- Optical Fiber Media is a dielectric material and not a metallic conductor
- Immune to electromagnetic interference
- No electromagnetic emissions (complies with EMC directives)
- No crosstalk between lines allows for secure data transmission
- Optical fibers and cables can be routed regardless of high power conductors
- Easy to handle (no special tools are required) and ideal for field installation
- Easy to operate, maintain, and repair
For POF-based communications, LEDs are still the predominant light source. Poly methyl methacrylate (PMMA) fiber has a 1 mm diameter core, which supports good transmission at 650 nm and a couple of windows around the green and blue wavelengths. The car industry, which is currently the biggest volume user of POF, is increasingly using LEDs and there is also a common low-speed industrial application area for measurement and control.
Flexibility
Key LED/POF communications system developer Avago Technologies offers a wide range of industrial fiber optic transceivers, transmitters, and receivers. Applications of these systems range from industrial automation, power generation and distribution, automotive communications, and medical systems to the booming gaming sector. Avago Technologies’ LEDs support communications in a variety of POF network types including automotive Polymer Optical Fiber, the widely-used industrial fieldbus-Sercos interface and general purpose, industrial control data links at 650 nm, 820 nm, and 1300 nm.
Industrial Fiber Optics² (IFO), based in Tempe, Arizona – home of Arizona State University – specializes in engineering, manufacture, and distribution of a variety of fiber optic products. Its core markets are the automation, factory drives, medical, and sensor industries. The company makes standard, custom and OEM fiber cable assemblies that utilize plastic and plastic-clad glass optical core fiber, bulk fiber cable, connectors, tools, and test equipment.
IFO recently expanded its SMA connector product line for plastic optical fiber. The new connectors boost the range of POF core diameters that can be linked. The latest SMA connectors are RoHS-compliant and designed for POF cable with either 0.5 mm or 0.75 mm optical cores. IFO’s existing connector range already accommodates standard POF cable with 1.0 mm fiber and 2.2 mm jackets.

Industrial Fiberoptics’ IF-E98³ is a high-speed, red LED housed in a connector-less style plastic fiber optic package. The output spectrum of the IF-E98 is produced by an Aluminum-Gallium-Arsenide (AlGaAs) die that peaks at a wavelength of 650 nm, which is one of the optimal transmission windows of PMMA plastic optical fiber. The device package features an internal micro-lens and a precision-molded PBT housing to ensure efficient optical coupling with standard 1000 μm core plastic fiber cable.
The short transition times of the IF-E98 make it suitable for medium-speed analog and digital data links. Link distances in excess of 75 m at data rates of 50 Mbit/s are possible using standard 1000 μm core plastic fiber when matched to IFO’s IF-D97 photologic detector. The drive circuit is simpler than required for laser diodes, making the IF-E98 a good, low-cost alternative in a variety of analog and digital communications applications.
Typical applications of IFO’s LED-based communications modules include: PC-to-peripheral data links, motor controller triggering, local area networks, automotive electronics, robotics communications and electronic gaming.
Lumex Industrial Communications
Lumex Industrial Communications4 also supports the full range of communications applications. Because the use of optoelectronics is expanding rapidly in the communications market, industrial customers with communications needs often seek a single supplier partner – such as Lumex – to ease the burden of sourcing multiple vendors.

Some of Lumex Industrial Communications’ focus niches within communications include: industrial network routing equipment, network security equipment, graphic processing units, computer equipment, storage area network equipment, enterprise servers, small to medium business phone systems, enterprise phone systems, microwave, optic and WiMAX equipment, and video conferencing equipment.
“Whether we are supporting standard SMT and through-hole LEDs or working on a fully integrated solution, our engineering design team is focused on ensuring that the end product being designed will fit the customer’s needs for the application, versus bending a product design to meet the components available,” as stated on the Lumex website. “We are always engaged with our customers to fine tune our offering and designs to meet their needs. We believe that design collaboration has consistently offered the best results for meeting the demands in the industrial controls environment and the increasing complexity of communications equipment designs.”
By partnering with a wide range of industrial control companies over many decades, Lumex has become a leading player in bringing new optoelectronic and display technology specifically designed for this market. A notable partner of Lumex is ROHM Semiconductor5, which offers a range of optical sensors and communication devices, from IR LEDs and phototransistors to fully integrated remote control receiver modules, IrDA transmitters, photo interrupters, and customized proximity sensor detectors.
ROHM Semiconductor’s IR LEDs and transistor sensor products are offered in packages ranging from standard T1, T11/4 packages to very small, low profile (0.9 mm) SMD top view and side view packages, all featuring ambient light resistance with wide or narrow viewing angles. These devices are suitable for remote control transmitters, games, security, industrial applications, and proximity detection.
ROHM Semiconductor’s IR receivers and IrDA communication devices with integrated LSI / IR components operate at low voltage and low power consumption while internal filters and shielding contribute to low noise operation and greater EMI resistance.
Trends and developments
Industrial networks have long been the mainstay of POF communications, commonly using LED sources, alongside Plastic Optical Fiber networks. A wide array of applications use POF, including machine control, sensing, networking and isolation, using both proprietary and standards-based protocols such as SERCOS, PROFIBUS or INTERBUS. These generally operate at speeds of up to 30 Mbit/s.
The most significant development in this market has been the recent decision by the association of German car manufacturers (AIDA) to move towards the utilization of the latest industrial Ethernet networking standard called PROFINET over Plastic Optical Fiber in their production plants. Such is the size of this industry that it has the potential to influence the adoption of this technology combination across a much wider range of industries, thus creating a long-term roadmap for optical-Ethernet-based networking standards across the entire industrial spectrum.
Conclusion
The market needs for POF are distinct and growing in terms of its usefulness and breadth of application. The need for solutions that bridge the gap between the cost benefits of copper and the performance benefits of fiber is clearly filled by POF. As each of the above mentioned ranges of products, applications, and associated markets continue to evolve, it is clear there is an appreciable need for higher speed industrial/data communications systems such as these based on POF and lit by LEDs, microlasers, vertical cavity surface emitting lasers, and other solid state sources.
References:
- Handbook of the European POF-Plus Project / Olaf Ziemann, Polymer Optical Fiber Application Center Nürnberg
- Industrial Fiber Optics
- Industrial Fiber Optics
- Lumex Industrial Communications
- ROHM Semiconductor
Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.