Point-of-Load Module Considerations

Przez: Aaron Yarnell

The endlessly creative art of marketing is a powerful tool that helps companies highlight their differentiations and advantages over industry competitors. The question is, do these supposed advantages make a difference in your particular application? Does it really matter if the product of interest is smaller-faster-stronger? As it turns out, like most things in life, the answer is “it depends”.

This article will attempt to look beyond typical marketing specifications to truly understand some of the key differences in point-of-load (POL) DC-DC converter performance and how they relate to your specific system design. Specifically, we will look at efficiency, output capacitance, compensation schemes, and cooling requirements.

Peak efficiency vs. efficiency under real-world loading conditions

The efficiency of power converters is typically denoted by the lowercase Greek letter, eta (η), and is expressed as the ratio of power delivered to the output relative to the power consumed by the input (η = Pout/Pin). The ideal ratio, or efficiency, of any converter is 1. This indicates that 100% of the power coming into the converter is delivered to the load with zero loss. In real-world applications, however, there will always be some loss/inefficiency associated with converting energy from one form to another and this will reduce the η from 1 down to something less.

Knowing that 100% efficiency is ideal, marketing teams often tout their highest achievable conversion efficiency possible in an attempt to stand out as the “best” for your application. This is often referred to as the “peak efficiency”. The challenge is that efficiency is not just a single number, but rather a multivariant function that is typically expressed as a function of output current/power delivered to the load. To illustrate how efficiency is affected by output load, below is a hypothetical example of a point-of-load efficiency curve:

Illustration of a typical efficiency curve

Figure 1:  Illustration of a typical efficiency curve.

In this hypothetical example, the peak of the efficiency curve occurs when the output load is at 50% of full load. At light loads the efficiency is much lower and at loads beyond the peak the efficiency gradually declines. It is important to understand these curves when you are designing a power delivery system because operating at any load above or below the peak efficiency point will result in wasted power and unwanted heat in your system. Below is an illustration showing that although POL B has the higher peak efficiency, POL A is the preferred choice for this application (in terms of efficiency) due to the amount of power demanded by the load.

Image of comparison of efficiency curves and loading conditions

Figure 2: Comparison of efficiency curves and application’s loading conditions.

Output capacitance required to achieve desired ripple/transient performance

Another metric of interest with POL converters is the amount of added system-level capacitance required to achieve your desired ripple and transient performance. The details surrounding the theory of external capacitor quantity and type are beyond the scope of this article, but it should be noted that not all POL modules are created equal when it comes to performance; even if the datasheets present similar numbers. On the surface it may appear that different POLs have similar ripple and transient performance, but if you dig deeper into the test conditions, you will often see big differences that can affect the overall cost and size of your power delivery solution.

Below is a comparison of two competing POL modules. From the data sheets’ high-level marketing bullet point numbers, these two potential solutions look to be fairly identical in terms of ripple and noise.

POL A POL B
Current Rating 60 A 40 A
Δ VOUT 10 mV 10 mV
Δ IOUT 30 A 20 A
Ceramic Capacitors 3x10 μF = 30 μF 4x47 μF = 188 μF
Polymer Capacitors 9x330 μF = 2970 μF 27x330 μF = 8910 μF
Total Capacitors ~3000 μF ~9000 μF

Figure 3: Output capacitance comparison between two POLs.

However, when analyzing the fine print we see that one of the modules (POL B) requires 300% more external capacitance to achieve the same voltage deviation performance as the other. This represents a significant amount of added cost and underutilized board space.

Fortunately, more advanced POL modules now offer full digital implementations, which afford significant improvement over traditional analog modules in terms of ripple/transient performance relative to the size of the overall solution.

The CUI NDM3Z-90 series is a great example of one such solution as it provides up to 90 amps of current to the load with superior ripple/transient performance, often with a significant reduction in output capacitance.

Image of NDM3Z-90 digital POL family from CUI

Figure 4: NDM3Z-90 digital POL family from CUI.

Compensation Schemes

A point-of-load module provides a stable and regulated output in an attempt to produce a clean voltage rail to its load. This implies that the POL inherently contains a negative feedback loop so that whenever a deviation from the ideal output occurs, the POL’s feedback network will compensate and attempt to bring the output back into ideal regulation.

There are many different nuanced compensation schemes available in the market, but below we will review the high-level strengths and weaknesses surrounding common analog and digital compensation schemes.

Analog Compensation: In an analog compensation network, the output of the module is sensed, filtered, and compared to a reference voltage to generate an error signal. This error signal is used to compensate the output and correct any deviations that may have occurred.

Schematic of a typical analog switching voltage regulator

Figure 5: Schematic of a typical analog switching voltage regulator.

The advantage with analog compensation schemes is that they have been around for a long time and can be implemented using standard off-the-shelf components. The drawback of these analog schemes is that it can be quite challenging to “tune the loop” to be stable across all operating conditions while maintaining a wide bandwidth for a fast transient response. This typically requires many hours in the lab soldering, testing, re-soldering, re-testing, etc. Analog compensation schemes are also susceptible to picking up external noise, which could inadvertently be coupled to the output.

Although the analog compensation scheme and its many variants have been the standard for quite some time, there are newer digital compensation schemes that have come along in the last decade or so, which offer some significant advantages.

Digital Compensation: Similar to analog schemes, a digitally-compensated implementation senses the output, filters it, compares it to a reference, generates an error, and ultimately compensates the output to correct any deviations that may have occurred.

Schematic of a typical digital switching voltage regulator

Figure 6: Schematic of a typical digital switching voltage regulator.

The major difference is all of this is done in the digital domain with 1’s and 0’s. The “sensing” of the output is done with an Analog-to-Digital converter and then all of the comparing, error-generation and compensation is done digitally inside an integrated circuit (IC). Operating within the digital domain also affords a significant improvement in noise rejection, which helps to prevent external noise sources from being inadvertently coupled to the output.

Utilizing a digital compensation scheme means you no longer have to spend hours in the lab soldering different components to tweak the feedback loop. Instead, you can simply modify a few digital parameters within the IC and change the behavior of the POL to meet the needs of your application. The more advanced digital POLs on the market today take this luxury one step further to offer “compensation-free” designs. In these designs the POL makes all of the necessary measurements and adjustments for you in-system to continuously provide a fast-reacting and stable output voltage rail.

Cooling requirements

One of the biggest limiting factors in point-of-load modules is heat dissipation. Inefficiencies in the module’s design results in unwanted internal heat generation causing critical components (e.g. FETs, inductors, capacitors, etc.) to approach their maximum rated operating temperature. Operation at or above these components’ thermal limits can reduce reliability and result in hardware failure.

To combat the damaging effects of internal heat generation, POL vendors often recommend a minimum amount of airflow to draw heat away from the module. This prevents heat from building up inside the components and raising temperatures beyond their rated limits. Using airflow to remove heat from the module can often increase the amount of power that can be delivered to the load and also improve the ambient operating temperature range. Below is an illustration showing a POL module’s ability to operate in different airflow environments ranging from natural convection (still air) to 3 m/s:

Illustration of a typical derating curve

Figure 7: Illustration of a typical derating curve under different airflow conditions.

We see that under natural convection (still air) conditions (denoted by the lowest solid line in Figure 7), the module can deliver 43 amps to the load up to 60°C. Adding just 2 m/s of airflow increases both the current capacity and ambient operating temperature range up to the full 50 A at 64°C ambient (denoted by the dash-dot line in Figure 7). However, forced-air cooling does have its drawbacks – it consumes power, which can negate some of the efficiency gains and can generate unacceptable levels of noise. Designers must carefully weigh the thermal requirements of the power module with the cooling capabilities of their system when selecting a POL.

Conclusion

Every application is different and values different performance metrics. For some, a fast transient response may be the most important consideration. Others may require the smallest size, highest efficiency, or widest operating temperature range. There is no one POL that can meet all of these requirements for each application no matter what the marketing teams may tell you. It is crucial to first understand your application’s needs under its specific operating conditions. Only then can you compare and select the optimal POL for your design.

 

Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.

Informacje o autorze

Aaron Yarnell

Article provided by Aaron Yarnell, Field Applications Engineering Manager, CUI Inc.