Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
LMX9838 Bluetooth Module Slide 6
Communication from the host processor is done over a standard high speed UART up to 921.6kbps. The host will send commands to the Simply Blue device and then return events confirm the results of the commands. These commands can be sent in two different modes, command or transparent. In Command Mode, the Simply Blue packet wrapper, which consists of header, operation codes, data and end delimiter, is interpreted and used to manage the connection between Bluetooth devices. This mode allows up to 7 active links at one time.
PTM Published on: 2011-11-02