Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
LMX9838 Bluetooth Module Slide 14
The LMX9838 includes the GAP, SDAP and SPP Bluetooth profiles. Additional profiles based on RFCOMM (i.e., DUN, FAX, OPP and FTP) can be implemented on the host processor. Since the module already supports the voice audio packet types, the HS and HF profiles can also be implemented with some additional code on the host processor. The Simply Blue developer’s site has application notes that describe the minimal software required for the host processor. It should be noted that the LMX9838 only includes certification for the GAP, SDAP and SPP profiles. Any additional profiles will need to be certified by the designer.
PTM Published on: 2011-11-02